LPC4088 I/O assignment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4088 I/O assignment

1,808 Views
grahamsewell
Contributor I

Hi, I am working with the LPC4088 and I have the EA mbed project as a start-point but I am trying to reallocate some of the I/O.  I can not find how the I/O is currently allocated e.g. how does a certain LCD driver pin get assigned to a particular function.  I have exported the mbed project to Keil uvision5 and this builds ok.

I have found parse_pins.cpp which contains the following:

#elif defined(TARGET_LPC4088_DM)
static const PinName pin_names[] = {p1, p2, p3, p4, NC, NC, p7, p8, p9, p10, p11, p12, p13, p14
, p15, p16, p17, p18, p19, p20, p21, p22, p23
, p24, p25, p26, NC, NC, p29, p30, NC, NC
, NC, NC, NC, NC, NC, NC, NC, NC, p41, p42, p43, p44, p45, p46};

but have not been able to rationalise this against the functionality.

Any help would be much appreciated.

Best wishes and good health to all!

Graham

Labels (2)
0 Kudos
Reply
1 Reply

1,750 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Graham Sewell,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the LPCOpen library to learn how to configure the I/O pin properly.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply