LPC4088 Developer's kit with USB mass storage device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4088 Developer's kit with USB mass storage device

2,032件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chrissweet on Sun Nov 09 13:45:35 MST 2014
Hi,
    I was hoping to get the LPC4088 Developer's kit working with the LPCOpen mass storage device example, unfortunately this seems to have been removed in version 2.xx of LPCOpen! Any way we can get this back? I would try the LPCOpen 1.3 library but the example has "/** Under development, not working yet. */#ifdef CFG_SDCARD" in SCSI.c so it doesn't inspire confidence. Anyone got anything like this working?

Best,
Chris

ラベル(1)
  • USB

0 件の賞賛
返信
3 返答(返信)

1,975件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chrissweet on Fri Dec 12 09:29:00 MST 2014
Thanks, I will look through this.

Best,
Chris
0 件の賞賛
返信

1,975件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chrissweet on Fri Dec 12 09:28:57 MST 2014
Thanks, I will look through this.

Best,
Chris
0 件の賞賛
返信

1,974件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Mon Dec 08 17:17:08 MST 2014
Meanwhile, you could reference the MSC example in below software package (it has both host and device examples):
http://www.lpcware.com/content/nxpfile/lpc407x-and-lpc408x-cmsis-compliant-standard-peripheral-firmw...
regards,
0 件の賞賛
返信