[LPC4088] Debugging problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[LPC4088] Debugging problem

1,259 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zbajchou on Sat Apr 25 09:32:55 MST 2015
Hi,

I have to program cheekers on LPC4088 with LCD but it is my first time with this device.
Could someone explain what mean:


Quote:
c:/nxp/lpcxpresso_7.7.2_379/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: emWin_516-test.axf section `.text' will not fit in region `MFlash512'
c:/nxp/lpcxpresso_7.7.2_379/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: region `MFlash512' overflowed by 56428 bytes



标签 (1)
0 项奖励
回复
2 回复数

1,210 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Apr 27 09:42:17 MST 2015
Hi,
The flash size of LPC4088 is 512KB. If you are unable to reduce the size and fit into this device  as suggested by R2D2. You may want to consider one of the below option.

Use QSPI flash to store data or slower code.

                    or
Use LPC1800 (M3, 1MB flash 180MHz speed ) see UM below

http://www.nxp.com/documents/user_manual/UM10430.pdf

                   or
Use LPC4300 (M4, 1MB Flash 204MHz speed) See UM below

http://www.nxp.com/documents/user_manual/UM10503.pdf
0 项奖励
回复

1,210 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat Apr 25 09:45:55 MST 2015
See: http://www.lpcware.com/content/faq/lpcxpresso/debug-build-too-big-fit-flash
0 项奖励
回复