LPC4078: using 16bit bus width external SDRAM as program memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4078: using 16bit bus width external SDRAM as program memory

2,032件の閲覧回数
otavioborges
Contributor III

Hello,

I'm developing an application using LPC4078FBD208 and an Alliance AS4C4M16SA SDRAM IC as external memory. After bootup I'm going to load the program data from a SD card, write it on the external memory and switch CPU context to execute from the external memory.

As M4 instructions are 32bit, the SDRAM 16bit bus width represent a problem for this scenario? The memory max clock is 144MHz, therefore I'll need two clock cycles (assuming that MCU core clock will be 120MHz) to fetch an entire instruction through EMC, will I have to reduce the CPU core clock to 60MHz to work with this setup?

Thank you.

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,828件の閲覧回数
carstengroen
Senior Contributor II

According to the users manual, the max EMC clock (I'm not 100% sure, but I read the "dynamic EMC timing" that Tmin is 12.5 nSec) is 80 MHz. I think you will have to set the EMC clock divider to 2 to get 60 MHz for the EMC if runinng the CPU at 120 MHz?  

0 件の賞賛
返信

1,828件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Otavio Borges ,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
As M4 instructions are 32bit, the SDRAM 16bit bus width represent a problem for this scenario? The memory max clock is 144MHz, therefore I'll need two clock cycles (assuming that MCU core clock will be 120MHz) to fetch an entire instruction through EMC, will I have to reduce the CPU core clock to 60MHz to work with this setup?
-- I don't think so.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信