LPC4078: using 16bit bus width external SDRAM as program memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4078: using 16bit bus width external SDRAM as program memory

2,016 次查看
otavioborges
Contributor III

Hello,

I'm developing an application using LPC4078FBD208 and an Alliance AS4C4M16SA SDRAM IC as external memory. After bootup I'm going to load the program data from a SD card, write it on the external memory and switch CPU context to execute from the external memory.

As M4 instructions are 32bit, the SDRAM 16bit bus width represent a problem for this scenario? The memory max clock is 144MHz, therefore I'll need two clock cycles (assuming that MCU core clock will be 120MHz) to fetch an entire instruction through EMC, will I have to reduce the CPU core clock to 60MHz to work with this setup?

Thank you.

标签 (1)
标记 (4)
0 项奖励
回复
2 回复数

1,812 次查看
carstengroen
Senior Contributor II

According to the users manual, the max EMC clock (I'm not 100% sure, but I read the "dynamic EMC timing" that Tmin is 12.5 nSec) is 80 MHz. I think you will have to set the EMC clock divider to 2 to get 60 MHz for the EMC if runinng the CPU at 120 MHz?  

0 项奖励
回复

1,812 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Otavio Borges ,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
As M4 instructions are 32bit, the SDRAM 16bit bus width represent a problem for this scenario? The memory max clock is 144MHz, therefore I'll need two clock cycles (assuming that MCU core clock will be 120MHz) to fetch an entire instruction through EMC, will I have to reduce the CPU core clock to 60MHz to work with this setup?
-- I don't think so.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复