LPC4078 Program Run in BootRom Area,could not jump to "main()"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4078 Program Run in BootRom Area,could not jump to "main()"

1,437件の閲覧回数
tangjianbo_cumt
Contributor I

无标题.png

1.png

When under debug mode , use Keil v5,program is always run in "0x1FFF01S2  4201  TST    ri,r0"  ,and this is BootRom . My program could not jump to Main().

The CPU is continue resting ??

ラベル(2)
0 件の賞賛
返信
1 返信

1,291件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, I'd like to learn more information about this 'issue'. Whether you can clarify these below inquires.
1) Sharing the Option for Target in Keil.
2) Which board and demo you.
3) The voltage status of the ISP pin.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信