LPC4078 FLASHCFG settings.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4078 FLASHCFG settings.

2,909件の閲覧回数
yangyu
NXP Employee
NXP Employee

Customer operated at 96 MHz CPU frequency with FLASHCFG register reset value 0x3(0011 Flash accesses use 4 CPU clocks. Use for up to 80 MHz CPU clock with power boost off (see Section 3.12.6).) and PBOOST register reset value 0x3(11 : Boost is on, operation up to 120 MHz is supported.).

Is this correct and safe settings?Thanks.

0 件の賞賛
返信
3 返答(返信)

2,890件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YuYang,

As the following figure, if you use 96MHz CPU clock, you can set the FLASHTIM bits as 0x100(5 cpu clocks with power boost off).

Power boost off can be set up as:

PBOOST=0x00;

I copy it here:

"0100 Flash accesses use 5 CPU clocks. Use for up to 100 MHz CPU clock with power boost off (see Section 3.12.6)."

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1608516052910.pngxiangjun_rong_0-1608516052910.png

Power boost control reg

xiangjun_rong_1-1608516519422.pngxiangjun_rong_1-1608516519422.png

 

 

 

 

0 件の賞賛
返信

2,887件の閲覧回数
yangyu
NXP Employee
NXP Employee

Hi Xiangjun,

Thanks for your reply.

In other word,with default reset value of FLASHTIM&Boost the cpu runs at 96MHz is unsafe?

In general,the designers don't notice these registers settings and just use the default value.Any official documents or sample codes to remind users?

0 件の賞賛
返信

2,882件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Yuyang,

Firstly, I do not think there is any documentation to remind user of the FLASHTIM&Boost registers.

Regarding your question whether it is safe to use the default FLASHTIM(3) and PBOOST(3) when the LPC4078 runs in 96MHz, I can not say it is safe or not.

I suggest you do a full temperature range test, if the chip runs okay in full temperature range especially in high temperature, it is okay.

BR

XiangJun Rong

0 件の賞賛
返信