LPC4078 ADC problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4078 ADC problem

1,915件の閲覧回数
albertoferrari
Contributor II

Hi everybody,

 

I'm using LPC4078 with LPCXpresso v8.1.4 (build 606).

 

I'm using 3 out of 8 ADC available on the LPC4078 (ADC0, ADC1 and ADC2) in burst mode.

 

It happens that sometimes, suddenly all the used ADCs tell me that the convertion has been done (DONE=1) but they give me 0 as result (even if the input voltage is about 0.5 volt).

 

Attacched you'll find the piece of code I used (here for debug I only check ADC0).

 

Do you have some hints about this issue?

 

Thanks in advance.

 

Alberto Ferrari

Original Attachment has been moved to: adc_lpc4078.c.zip

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,644件の閲覧回数
Dezheng_Tang
NXP Employee
NXP Employee

Alberto,

    If you do a burst on three channels, you need to make sure all channels have finished conversion, your code only checked ADC0 DONE bit. You can check STAT bit 0~2 and make sure all of them are set and no OVERRUN on any of these channels.

0 件の賞賛
返信

1,644件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Alberto,

Could you please test the ADC example located at the path C:\nxp\LPCXpresso_8.1.4_606\lpcxpresso\Examples\LPCOpen ? This is in order to isolate the issue. I want to know if there is a hardware or software issue.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信