LPC32xx trying to get Standard UART Rx interrupt after single byte

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC32xx trying to get Standard UART Rx interrupt after single byte

1,589 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brothwell on Tue Sep 18 09:32:15 MST 2012
Am a bit confused by the interrupt behavior of the standard UART (specifically UART 3) on the LPC32xx.

Effectively, I would like to have a large receive FIFO with a > 0 byte interrupt trigger.  The documentation implies that a CTI / RDA interrupt is the correct mechanism, but I don't see an obvious way to configure that. 

Can someone clear up my confusion?

Thanks in advance,
Brian
Labels (1)
0 Kudos
Reply
1 Reply

1,581 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brothwell on Fri Sep 21 07:19:24 MST 2012
Someone reported on another forum that they were getting the behavior I was looking for. Setting FCR register to zero seems to produce the right behavior.

Consider this issue dead.
0 Kudos
Reply