LPC3250 boot without UART5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC3250 boot without UART5

1,882 Views
lllggg000111
Contributor I

In my LPC3250 development board, I did not connect the UART5, how can I boot?Is there any other way to burn the program?I have USB,hsuart1/2,nandfalsh.

Labels (1)
0 Kudos
Reply
2 Replies

1,609 Views
lllggg000111
Contributor I

Thanks for your answer!

0 Kudos
Reply

1,609 Views
b36401
NXP Employee
NXP Employee

LPC3250 can boot also from NAND Flash and SPI.
Please refer chapter 35 "LPC32x0 Boot process" of LPC32x0 user manual.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply