LPC3250 boot without UART5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC3250 boot without UART5

1,948 次查看
lllggg000111
Contributor I

In my LPC3250 development board, I did not connect the UART5, how can I boot?Is there any other way to burn the program?I have USB,hsuart1/2,nandfalsh.

标签 (1)
0 项奖励
回复
2 回复数

1,675 次查看
lllggg000111
Contributor I

Thanks for your answer!

0 项奖励
回复

1,675 次查看
b36401
NXP Employee
NXP Employee

LPC3250 can boot also from NAND Flash and SPI.
Please refer chapter 35 "LPC32x0 Boot process" of LPC32x0 user manual.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复