LPC3250 boot without UART5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC3250 boot without UART5

1,910件の閲覧回数
lllggg000111
Contributor I

In my LPC3250 development board, I did not connect the UART5, how can I boot?Is there any other way to burn the program?I have USB,hsuart1/2,nandfalsh.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,637件の閲覧回数
lllggg000111
Contributor I

Thanks for your answer!

0 件の賞賛
返信

1,637件の閲覧回数
b36401
NXP Employee
NXP Employee

LPC3250 can boot also from NAND Flash and SPI.
Please refer chapter 35 "LPC32x0 Boot process" of LPC32x0 user manual.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信