LPC29xx Peripheral Library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC29xx Peripheral Library

1,647 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TahaSN on Tue Mar 10 09:36:41 MST 2015
Hello,

I am planning to use LPC2929 (or other in similar series) microcontroller for my upcoming project. I am not able to find LPC29xx Code Library from LPC-Open or somewhere else which can help me kickstart my project. Does it count in LPC2000 Series? If not then can anyone direct me to correct location.

Thanks,
Taha
标签 (1)
0 项奖励
回复
2 回复数

1,604 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TahaSN on Tue Mar 10 11:08:02 MST 2015
Thanks for your quick reply.

Good to know. I look into Cortex-M class then.
0 项奖励
回复

1,604 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Mar 10 10:37:07 MST 2015
First off - I would recommend that consider using a Cortex-M class part instead of LPC29xx, which are now pretty old.

But that aside, the example code base for LPC29 seems to have disappeared off the web. The only available code I can find are:

- an example project within the LPCXpresso examples
- An example on the Hitex website : http://www.hitex.co.uk/index.php?id=2177

Regards,
LPCXpresso Support
0 项奖励
回复