LPC29xx Peripheral Library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC29xx Peripheral Library

1,676件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TahaSN on Tue Mar 10 09:36:41 MST 2015
Hello,

I am planning to use LPC2929 (or other in similar series) microcontroller for my upcoming project. I am not able to find LPC29xx Code Library from LPC-Open or somewhere else which can help me kickstart my project. Does it count in LPC2000 Series? If not then can anyone direct me to correct location.

Thanks,
Taha
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,633件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TahaSN on Tue Mar 10 11:08:02 MST 2015
Thanks for your quick reply.

Good to know. I look into Cortex-M class then.
0 件の賞賛
返信

1,633件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Mar 10 10:37:07 MST 2015
First off - I would recommend that consider using a Cortex-M class part instead of LPC29xx, which are now pretty old.

But that aside, the example code base for LPC29 seems to have disappeared off the web. The only available code I can find are:

- an example project within the LPCXpresso examples
- An example on the Hitex website : http://www.hitex.co.uk/index.php?id=2177

Regards,
LPCXpresso Support
0 件の賞賛
返信