LPC2478 Read cycle OE width

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2478 Read cycle OE width

68 Views
KumarBax
Contributor I

Observing almost double the OE width for below settings on LPC2478 processor. Is it common? Why?

EMCStaticConfig0         -  0x81
EMCStaticWaitOen0      - 0
EMCStaticWaitRd0        - 4
EMCStaticWaitPage0    - 0
EMCStaticWaitWr0       - 3
EMCStaticWaitTurn0    - 0

CCLK        - 51.6 Mhz
HCLK        - 51.6 Mhz
EMCCLK   - 51.6 Mhz

Labels (1)
0 Kudos
Reply
1 Reply

43 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @KumarBax 

EMCStaticConfig0 = 0x81 configures the static memory interface as 16-bit.

With EMCStaticWaitRd0 = 4 and EMCStaticWaitOen0 = 0, the nominal read interval is five CCLK periods. At 51.6 MHz, this corresponds to approximately:

5 × 19.38 ns ≈ 96.9 ns

The measured OE-low interval of approximately 193 ns is close to ten CCLK periods. One possible explanation is that the measured interval covers more than one external memory transfer. For example, if the processor performs a 32-bit read through the 16-bit EMC interface, two 16-bit transfers would be required, resulting in approximately:

2 × 96.9 ns ≈ 193.8 ns

However, the OE waveform alone is not sufficient to confirm this.

Could you please check the instruction/access width that generated this waveform? As a further verification, you could compare explicit 16-bit and 32-bit reads while monitoring OE, CS, and the address lines.

BR

Harry

0 Kudos
Reply