LPC2478 LCD clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2478 LCD clock

2,773 Views
sivaramakrishna
Contributor I

HI,

I have configured the LPC2478 LCDDCLK clock to 24MHz O/P and observed that the clock is not reaching to full 0VDC on the negative transition.

I have made the following measurements and observe the issue:

1) Configured the DCLK at Pin 150 to 14MHz and observed the sine wave clk  with slow rise and fall times.

2) When it is configured to 24MHz clock the clock signal is not  reaching to complete 0VDC on the negative transition.

Can you please suggest the root cause and possible trouble shooting techniques on this.Measurement WF are attached for reference.

Thanks ,

Siva Bommaraju

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,607 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Siva,

If you are using a custom board, you should verify the general design recommendations for clock signals, as it seems to be hardware related (i.e. unbalanced impedances/capacitances).

As complementary information, you could take a look to the following links:

https://www.nxp.com/docs/en/application-note/AN10778.pdf

http://www.onarm.com/forum/20290/


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply