LPC2470 usb bootloader for Windows10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2470 usb bootloader for Windows10

2,389 次查看
pandiayn8696
Contributor I

Hi , I am using LPC2470 in one of our project and we have developed the usb bootloader for field upgrade . We developed the bootloader based on AN10764 (USB secondary ISP bootloader for LPC24xx ) . It was working well for all Windows platform except Windows 10 . Windows 10 actually identify the device and i could see the folder but not able to open the folder to copy the bin file . 

Hope some of you might have faced the same issue and awaits to get a support from experts to solve the issue. 

Thanking you , 

Pandiyan.

0 项奖励
回复
2 回复数

2,330 次查看
pandiayn8696
Contributor I

Hello Sabina, 

Thanks for your prompt reply , I followed the steps to disable the Windows 10 driver signature permanently . But , the issue is still persist . Do you think this is the issue with drivers signature ?

Hope to get get some advise on this issue  

Regards,

Pandiyan .

0 项奖励
回复

2,330 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello Pandiyan,

Hope you are doing well.

The LPC24xx is part of the legacy devices and it has limited support.

I recommend that you try to disable the Secure Authentication feature of Windows 10.

Driver Signing Changes in Windows 10

How to disable driver signature permanently

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 项奖励
回复