LPC2468

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2468

11,483件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Italia on Sat Jun 14 05:12:56 MST 2014
Hi,

i'm loocking for LPC2468 svd file. Can someone help me? I look on the site but i haven't found it.

Thank to everyone!
ラベル(1)
0 件の賞賛
返信
32 返答(返信)

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Italia on Mon Jun 16 09:02:39 MST 2014
Sorry, i'm using J-LINK probe on my custom hardware.
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 16 08:49:41 MST 2014
You didn't answer my question. Which Debug Probe?

As you can see from the attachment, on my computer, using LPC-Link, LPC-Link2, CMSIS-DAP or Red Probe, then I can view all of the Peripherals and the Timer1 peripheral details.
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Italia on Mon Jun 16 08:42:37 MST 2014
I can't view any register. Supposing that i want look IR register of TIMER1, i can watch it only loocking to 0xE000 8000 memory location??
There is not in the ide the possibilities to watch the register name associtated to the peripheral?
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 16 07:48:35 MST 2014
Which debug probe? Which peripheral? Which register?
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Italia on Mon Jun 16 07:42:09 MST 2014
In this moment i'm tring to debug with LPCXpresso trial edition. I uploaded a test program on the CPU, but when enter in degug, I can not see the device register value cause the peripheral windows is empty and do not contain the processor register.
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 16 07:24:51 MST 2014
Sorry, I don't understand what you are trying to do. Can try explaining again? Please explain what it is you cannot do in LPCXpresso.
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Italia on Mon Jun 16 05:58:39 MST 2014
I need an environment that give me the possibilities to watch the peripherals register, so i try LPCXpresso but seem
it not allow to view peripherals stored value. For thes reason i try other IDE, that have the same problem.
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 16 05:44:46 MST 2014
No, LPCXpresso does not use an SVD file for generating the Peripheral view for LPC2000 family parts. And there is no SVD file for these parts anyway. These parts predate the SVD format, and we are not planning to go back and create them

What are you actually trying to do?

Regards,
LPCXpresso Support
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Italia on Mon Jun 16 05:28:26 MST 2014
Also the LPCXpresso IDE need the svd file or the peripheral have readed in other way?
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sat Jun 14 09:47:53 MST 2014
Lpc1768 is similar.
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Italia on Sat Jun 14 05:53:22 MST 2014
Are there some processor that have a similar svd file?
0 件の賞賛
返信

3,068件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sat Jun 14 05:25:47 MST 2014
There is no such thing. Svd is for cortex-m devices, and afaik, nobody has back ported to,these old arm7 based devices.
0 件の賞賛
返信