LPC2468 Secondary Bootloader - Enter supervisor mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2468 Secondary Bootloader - Enter supervisor mode

ソリューションへジャンプ
2,059件の閲覧回数
NilsDrotleff
Contributor II

Hey there,

I am currently developing a secondary bootloader (SBL) for updates of the LPC2468 via an arbitrary UART. Everything is working fine, except the jump to the user application out of the SBL.

This is due to the user mode the processor is in at the time of the jump. Hence the stackpointers and some other stuff won't be set correctly in the startup file of the application.

My workaround would be, to check the entry conditions for the SBL in the startup file, while still in supervisor mode. This isn't supposed and makes it a little complicated, e.g. to check if a correct application is even existing.

Is there a way to first enter the SBL, then check the entry conditions for the ISP mode and if a jump to the application is required set the processor in supervisor mode again? A reset at every startup after entering the SBL and before jumping into the application is not applicable.

Thanks in advance

Nils 

0 件の賞賛
返信
1 解決策
2,047件の閲覧回数
NilsDrotleff
Contributor II

I have used the Startup file to switch between SBL and application. Inserted the code below at the beginning of the reset handler:
Possibly not the best assembly code in this world, but it works.

; ----------------------------------------------------------------------
; ----------------- Check if SBL entry is required ---------------------
; ----------------------------------------------------------------------
; constants
SblFlag_TRUE EQU 0x12345678
CRP3 EQU 0x43218765
Address_CRP EQU 0x1FC ; word
Address_SBLFLAG EQU 0x7000 ; word
AddressStart_APP EQU 0x8000
AddressEnd_BLANKCHECK EQU 0xFFFF

; Check if user code is present
; if user code not present, branch to sbl entry
LDR R0, =AddressStart_APP
LDR R1, =AddressEnd_BLANKCHECK

; loop first sector of app area
loop_start ; load first byte
LDRB R2, [R0]
; Check if byte is empty (0xFF)
CMP R2, #0xFF
; break loop and check other conditions
BNE app_present

; check if actual address equals end of sector
; subtract actual address from final address
; SUBS sets the Z flag if equal
SUBS R3, R1, R0
; if result is zero
; end loop and branch to SBL, because no code is present
BEQ enter_sbl

; increment address
ADD R0, R0, #1

; branch to next iteration (check next byte)
B loop_start


app_present ; Load registers for CRP3 check
LDR R0, =Address_CRP
; Load word value from Address_CRP
LDR R0, [R0]
LDR R1, =CRP3

; check if CRP3 is enabled
; SUBS sets the Z flag if equal
SUBS R2, R0, R1

; if CRP3 is enabled AND user code is present
; branch to application
BEQ enter_app

; Load registers for SBL flag check
LDR R0, =Address_SBLFLAG
; Load word value from Address_SBLFLAG
LDR R0, [R0]
LDR R1, =SblFlag_TRUE

; check if sbl flag is set
; SUBS sets the Z flag if equal
SUBS R2, R0, R1

; if sbl flag set, branch to sbl
; else branch to application
; (User code present check was alreay performed)
BEQ enter_sbl

; Branch to main / user application
enter_app LDR R0, =AddressStart_APP
BX R0

; branch to SBL if user code not present
; OR
; CRP3 not enabled AND SBL flag set
enter_sbl

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,047件の閲覧回数
NilsDrotleff
Contributor II

I have used the Startup file to switch between SBL and application. Inserted the code below at the beginning of the reset handler:
Possibly not the best assembly code in this world, but it works.

; ----------------------------------------------------------------------
; ----------------- Check if SBL entry is required ---------------------
; ----------------------------------------------------------------------
; constants
SblFlag_TRUE EQU 0x12345678
CRP3 EQU 0x43218765
Address_CRP EQU 0x1FC ; word
Address_SBLFLAG EQU 0x7000 ; word
AddressStart_APP EQU 0x8000
AddressEnd_BLANKCHECK EQU 0xFFFF

; Check if user code is present
; if user code not present, branch to sbl entry
LDR R0, =AddressStart_APP
LDR R1, =AddressEnd_BLANKCHECK

; loop first sector of app area
loop_start ; load first byte
LDRB R2, [R0]
; Check if byte is empty (0xFF)
CMP R2, #0xFF
; break loop and check other conditions
BNE app_present

; check if actual address equals end of sector
; subtract actual address from final address
; SUBS sets the Z flag if equal
SUBS R3, R1, R0
; if result is zero
; end loop and branch to SBL, because no code is present
BEQ enter_sbl

; increment address
ADD R0, R0, #1

; branch to next iteration (check next byte)
B loop_start


app_present ; Load registers for CRP3 check
LDR R0, =Address_CRP
; Load word value from Address_CRP
LDR R0, [R0]
LDR R1, =CRP3

; check if CRP3 is enabled
; SUBS sets the Z flag if equal
SUBS R2, R0, R1

; if CRP3 is enabled AND user code is present
; branch to application
BEQ enter_app

; Load registers for SBL flag check
LDR R0, =Address_SBLFLAG
; Load word value from Address_SBLFLAG
LDR R0, [R0]
LDR R1, =SblFlag_TRUE

; check if sbl flag is set
; SUBS sets the Z flag if equal
SUBS R2, R0, R1

; if sbl flag set, branch to sbl
; else branch to application
; (User code present check was alreay performed)
BEQ enter_sbl

; Branch to main / user application
enter_app LDR R0, =AddressStart_APP
BX R0

; branch to SBL if user code not present
; OR
; CRP3 not enabled AND SBL flag set
enter_sbl

0 件の賞賛
返信