LPC2388 Toggling *SSEL when using SSP0 for SPI communications

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2388 Toggling *SSEL when using SSP0 for SPI communications

6,411件の閲覧回数
perdrix
Contributor II

Reading Chapter 19 (SSP ...) of the User Manual, my understanding of the usage is that I should configure to use SSP0 (say) as SPI, and then use code similar to this:

void SSP_SPI_SR(uint16_t* sendBuffer, uint16_t* recvBuffer, uint8_t length)
{
     uint8 len1 = length, len2 = length;
     
     // Ensure SSP receive FIFO is empty (by reading data out of it if necessary)
     while(SSP0SR & RNE) SSP0DR;

     IOCLR0 = 0x00100000;  // SSEL active (down)
     while(len1 || len2)
     {

           if (len1 && (SSP0SR & TNF)) // Data to send and transmit FIFO isn’t full?
           {
                SSPODR = *sendBuffer++;
                len1--;
                //
                // add a wait loop here if need to prevent buffer underrun at slave
           }
           
           if (len2 && (SSP0SR & RNE)) // Data to receive and receive FIFO has data available
           {
                *recvBuffer++ = SSP0DR;
                len2--;
           }

     }
     
     }
     IOSET0 = 0x00100000;  // SSEL inactive (up)
}

// Usage :

uint16_t pollSequence[9] = {0xEBEB, 0xEBEB, 0xEBEB,
                0xEBEB, 0xEBEB, 0xEBEB,
                0xEBEB, 0xEBEB, 0xFFFF};   

uint16_t pollReplies[9] = {0};

SSP_SPI_SR(pollSequence, pollReplies, 9);

 Is that right?

If so I'm puzzled! Using CPOL=1, CPHA=0. Section 19.5.2.4 explicitly says:

However, in the case of continuous back-to-back transmissions, the SSEL signal must be
pulsed HIGH between each data word transfer. This is because the slave select pin
freezes the data in its serial peripheral register and does not allow it to be altered if the
CPHA bit is logic zero. Therefore the master device must raise the SSEL pin of the slave
device between each data transfer to enable the serial peripheral data write. On
completion of the continuous transfer, the SSEL pin is returned to its idle state one SCK
period after the last bit has been captured.

But given that the FIFO is being used for data transmission, I don't understand how I am supposed to toggle *SSEL between transfers.

Help greatly appreciated.

Thanks, David

0 件の賞賛
返信
12 返答(返信)

3,501件の閲覧回数
butmanufacturer
Contributor II

This communication converter I have applied to make video streaming app and it is awesome, HDO Box app is available for android, ios, firestick, pc and smart tv. Download it at HDO Box website

0 件の賞賛
返信

5,543件の閲覧回数
hdobox
Contributor I

Here is the best and latest sreaming application HDO box is the free app. HDO Box provide new movies for all time

0 件の賞賛
返信

6,288件の閲覧回数
perdrix
Contributor II

Think about this please.   Not a single reply has addressed the issue that I'm adding messages to a FIFO queue to be sent, and I cannot control when they are sent, and there's no obvious way to toggle *SSEL between the transmission of one message and the next.

0 件の賞賛
返信

6,253件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

please test below code if possible: 

 

void SSP0Send( BYTE *send_buf, BYTE *recv_buf, DWORD Length )
{
  DWORD i;
  BYTE Dummy = Dummy;
   
  for ( i = 0; i < Length; i++ )
  {
  /* Move on only if NOT busy and TX FIFO not full. */
  while ( (SSP0SR & (SSPSR_TNF|SSPSR_BSY)) != SSPSR_TNF );
  SSP0DR = *send_buf;
  send_buf++;
 
  while ( (SSP0SR & (SSPSR_BSY|SSPSR_RNE)) != SSPSR_RNE );
  /* Whenever a byte is written, MISO FIFO counter increments, Clear FIFO
  on MISO. Otherwise, when SSP0Receive() is called, previous data byte
  is left in the FIFO. */
  *recv_buf = SSP0DR;
  recv_buf++
 
  /* Wait until the Busy bit is cleared. */
  while ( SSP0SR & SSPSR_BSY );
  }
  return;
}
 
 
please also intialize the SSEL pin as GPIO with output mode.
 
BR
Alice

 

0 件の賞賛
返信

6,339件の閲覧回数
perdrix
Contributor II

Please apply the little grey cells here and read my code snippet and quote from the manual.   The messages to be transmitted are in the transmit FIFO and I have no control over when they are sent, and AFAICT no way to toggle *SSEL between messages.   If there's a relevant code in the SSP sample I didn't see it so please point me to the relevant line of code (clearly I know how to manipulate *SSEL before putting messages into the xmit FIFO).

0 件の賞賛
返信

6,291件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

Try to config the SSEL pin as gpio function, then set to high or low.

 

 

BR

Alice

0 件の賞賛
返信

6,357件の閲覧回数
perdrix
Contributor II

Still looking for an answer

 

D.

0 件の賞賛
返信

6,379件の閲覧回数
fincherdavid
Contributor I

I am referring to document UM10211 which is the official User Manual for the LPC2388:

LPC23XX User manual

Thanks for the pointer to the NXP forums I have posted there.

0 件の賞賛
返信

6,382件の閲覧回数
perdrix
Contributor II

Alice, I downloaded the code samples some time ago.  Please could I ask that you point me to the relevant sample that covers this specific question, as I didn't find one that seemed relevant.

Thanks, David

0 件の賞賛
返信

6,344件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello David,

I'm not familiar wit this chip, I meaning you can refer to the ssp  demo under Sample Code Bundle.

 

BR

Alice

0 件の賞賛
返信

6,398件の閲覧回数
perdrix
Contributor II

Anyone know the answer?

0 件の賞賛
返信

6,388件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

How about refer to demo code how to config: 

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...  

Alice_Yang_0-1645520085794.pngAlice_Yang_0-1645520085794.png

 

 

BR

Alice