LPC2388 MAC address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2388 MAC address

2,566件の閲覧回数
mohammadfaizan
Contributor III

Hi,

I am working on a project, which has a one module of TCPIP  communication. But before I had used a PIC32 microchip controller which is shipped with a in-build mac address, what in case of LPC2388  and LPC1788, does it have a in-build mac address  or I need to assign,  how I can assign the unique mac address.

thanks & regards

Mohammad Faizan

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

2,386件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Mohammed

The MAC-address can be entered via the 'Station Addresses'.
See User Manual UM10211. Search on 'Station Address'.

See: http://www.lpcware.com/content/nxpfile/lpc23xx-user-manual


But (...) NXP does not supply MAC addresses for its products. The only way, I see, is to buy them from the IEEE:
 
http://standards.ieee.org/regauth/oui/index.shtml
https://standards.ieee.org/regauth-bin/application?rt=OUI
 
You buy a block of 16 million addresses, and that currently costs you (?)  $1825.

There is an Application Note handeling about connecting the LPC2000 with ethernet, see:

http://www.lpcware.com/content/nxpfile/an10403-connecting-ethernet-interface-lpc2000

2,386件の閲覧回数
mohammadfaizan
Contributor III

Thanks Jamesbone

0 件の賞賛
返信