LPC2388 - Can I use a GPIO instead of VBUS to detect the presence of a USB host?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2388 - Can I use a GPIO instead of VBUS to detect the presence of a USB host?

921 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wwwenrico on Thu Apr 14 07:11:17 MST 2016
Hello,


I designed a board, based on the LPC2388, with an USB device interface.



The VBUS (pin P1.30) is used as an ADC and not as a VBUS detector.



QUESTION 1
Can I use a GPIO pin to detect the status of the VBUS?



QUESTION 2
Which software corrections I have to do to Keil HID demo program?



Thanks,
Enrico Migliore
Labels (1)
0 Kudos
Reply
1 Reply

840 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply