LPC2388 - Can I use a GPIO instead of VBUS to detect the presence of a USB host?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2388 - Can I use a GPIO instead of VBUS to detect the presence of a USB host?

920件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wwwenrico on Thu Apr 14 07:11:17 MST 2016
Hello,


I designed a board, based on the LPC2388, with an USB device interface.



The VBUS (pin P1.30) is used as an ADC and not as a VBUS detector.



QUESTION 1
Can I use a GPIO pin to detect the status of the VBUS?



QUESTION 2
Which software corrections I have to do to Keil HID demo program?



Thanks,
Enrico Migliore
ラベル(1)
0 件の賞賛
返信
1 返信

839件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信