LPC2387 interface with MM74HC573 - 3 state problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2387 interface with MM74HC573 - 3 state problem

804 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Erez on Thu Sep 24 02:18:16 MST 2015
Hi,
Im using P1[17] as out_control for MM74HC573.
When i first connect the voltage or reset the system, i am getting voltage 2[v] ( ONly voltage above 3[v] means '1')
This is a big problem. i need the value to be '1' (or '0').
How can i solves this?

I've tried some actions:
- Disabled the P1[17]  ENET-MDIO option
- Tried to write directly to the register- no effect
- Tried to connect pull up resistor.

Could someone help in this please?

By the way,
I have already a system that works perfect when i use the P0[26] for outcontrol.
标签 (1)
0 项奖励
回复
0 回复数