LPC2368 + external RAM (61LV256AL)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2368 + external RAM (61LV256AL)

2,235 Views
pazdimpazdim
Contributor II

Hello. I'm looking for an external RAM for LPC2368. My choice - IS61LV256AL. Can I use GPDMA to access external memory? How much it fast and difficult? Thank you.

Labels (3)
0 Kudos
Reply
2 Replies

2,065 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

If you are developing a new application, you may consider a newer option, as the LPC2xxx are now part of the legacy devices. Anyway, in case of requiring external RAM, as the LPC2368 doesn’t have external memory controller, there are some cases where external SRAM can be connected with GPIOs, just considering the address, data pins status/impedances. As it may become slow/difficult, another option could be using an external I2C or SPI RAM, using these peripherals already included on the LPC2368.

Hope this will be useful for you.

Best regards!

/Carlos

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,065 Views
pazdimpazdim
Contributor II

Does the RAM connect to the GPIO?

0 Kudos
Reply