LPC2368 + external RAM (61LV256AL)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2368 + external RAM (61LV256AL)

2,256 次查看
pazdimpazdim
Contributor II

Hello. I'm looking for an external RAM for LPC2368. My choice - IS61LV256AL. Can I use GPDMA to access external memory? How much it fast and difficult? Thank you.

标签 (3)
0 项奖励
回复
2 回复数

2,086 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

If you are developing a new application, you may consider a newer option, as the LPC2xxx are now part of the legacy devices. Anyway, in case of requiring external RAM, as the LPC2368 doesn’t have external memory controller, there are some cases where external SRAM can be connected with GPIOs, just considering the address, data pins status/impedances. As it may become slow/difficult, another option could be using an external I2C or SPI RAM, using these peripherals already included on the LPC2368.

Hope this will be useful for you.

Best regards!

/Carlos

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,086 次查看
pazdimpazdim
Contributor II

Does the RAM connect to the GPIO?

0 项奖励
回复