LPC2368 - USBHwEPWrite doesn't write on SIE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2368 - USBHwEPWrite doesn't write on SIE?

921件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cyba on Fri Sep 04 08:32:47 MST 2015
Hi, I have a problem with a project based on the LPC2368  micro and the LPCUSB stack (the same stack used on the CMSIS2 examples for the LPC17xx family too).
The project makes a custom USB communiction with a Windows application in the host PC, using 4 Bulk Endpoint (2 IN and 2 Out). Everithing work well with USB2.0 ports on all windows o.s. and different USB mainboard hardware, but with USB3.0 ports the communication hangs.
With USB3.0 the device is correctly enumerated, windows load the right driver and the host application starts the communication sending a command to the LPC2368 with a BulkOut endpoint message, I've found that the problem is with a USBHwEPWrite function that should answer to this command: the USBHwEPWrite seems to write the data buffer to the SIE but with a USB sniffer I can't see the message (and the host app also crash).
This is a part of code to explain what I mean ( BULK_CMD_IN_EP 0x82, BULK_CMD_OUT_EP 0x05), the function GetUSBCmd() is called in the BULKOUT handler:
void GetUSBCmd(void)
{
       /* here I receive the host command */
iLen = USBHwEPRead(BULK_CMD_OUT_EP, abBulkBuf, sizeof(abBulkBuf));
        if( .... ) {
        /*
            here I make some controls on the command received from the host
            and If it is correct I reply with a confirmation message that I send here after
*/
   iLen = USBHwEPWrite(BULK_CMD_IN_EP, abBulkBuf, 0x10);
}
}


Just to understand what happen I've traced the status of the EP with some debug string messages and i've found that with USB3.0 after the USBHwEPWrite instruction the count of transferred bytes iLen seems to be correct but I can't see any message on the usb (checked with a sniffer).
Also I've tryied to analyze the EP status with  the instruction:
EPStatus = USBHwEPGetStatus(BULK_CMD_IN_EP);
but I have some problems with the meaning of the reported answer (maybe I'm just stupid but I can't find this info on LPC2368 manual)...
Someone has any idea or can help me with this issue?
thanks!
Cyba
ラベル(1)
0 件の賞賛
返信
1 返信

901件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cyba on Mon Sep 21 01:15:01 MST 2015
Hello, nobody can help me?
I'll try with another question:
has anybody experience with LPC23xx micro and the LPCUSB stack (Bulk endpoint transfer) interfacing with USB3.0 host computers?
thanks!
0 件の賞賛
返信