LPC2366 SDK and DEBUG Link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2366 SDK and DEBUG Link

1,398 Views
dennisgriffin
Contributor I

I'm looking for an SDK for the LPC2366?

i'm also wondering if the debug link on the LPC55S69-EVK will work with the LPC2366?

0 Kudos
Reply
3 Replies

1,326 Views
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, there is no SDK for the LPC2366.

In addition, this device is not recommended for new designs.

Regards 

Soledad

0 Kudos
Reply

1,326 Views
dennisgriffin
Contributor I

Thanks.

as a test eng. i don't get to pick the part i have to test...lol

Dennis G.

0 Kudos
Reply

1,326 Views
bernhardfink
NXP Employee
NXP Employee
  • The LPC2366 has an ARM7TDMI, the debugger bridge on the LPC55x boards will not work because it is made for debugging Cortex-M based MCUs.
  • You need a SEGGER j-Link, a KEIL ULINK or something like that.
  • If you install the older LPCXpresso Tool, then you can generate a project for the LPC2366. MCUXpresso does not support it.
  • For this MCU generation we had so called "Code Bundles" for KEIL µVision IDE, see attachment

Regards,

Bernhard.

0 Kudos
Reply