LPC2366 SDK and DEBUG Link

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2366 SDK and DEBUG Link

2,058件の閲覧回数
dennisgriffin
Contributor I

I'm looking for an SDK for the LPC2366?

i'm also wondering if the debug link on the LPC55S69-EVK will work with the LPC2366?

0 件の賞賛
返信
3 返答(返信)

1,986件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, there is no SDK for the LPC2366.

In addition, this device is not recommended for new designs.

Regards 

Soledad

0 件の賞賛
返信

1,986件の閲覧回数
dennisgriffin
Contributor I

Thanks.

as a test eng. i don't get to pick the part i have to test...lol

Dennis G.

0 件の賞賛
返信

1,986件の閲覧回数
bernhardfink
NXP Employee
NXP Employee
  • The LPC2366 has an ARM7TDMI, the debugger bridge on the LPC55x boards will not work because it is made for debugging Cortex-M based MCUs.
  • You need a SEGGER j-Link, a KEIL ULINK or something like that.
  • If you install the older LPCXpresso Tool, then you can generate a project for the LPC2366. MCUXpresso does not support it.
  • For this MCU generation we had so called "Code Bundles" for KEIL µVision IDE, see attachment

Regards,

Bernhard.

0 件の賞賛
返信