LPC2362 Not entering ISP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2362 Not entering ISP mode

1,194件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jaisankar_av on Thu Jul 04 00:05:01 MST 2013

Hi,


I have a strange problem with my board LPC2362. The fresh controller is getting programmed for the very first time. And the second time onwards the controller is not entering into ISP mode.


I am using Flash magic for programming. RTS and CTS are included in the ISP connections and using via PC serial port.


I have probed the Reset pin and EINT(P2.10). Both are going LOW initially and then HIGH when trying to connect from flash magic, though not connecting on second attempt. The error I get is Failed to Autobaud.


First time after changing the controller, it works fine. So the ISP circuit is fine I guess.


Any valuable suggessions would be highly appriciated.


Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,155件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by barny on Wed Dec 04 01:49:26 MST 2013
Hi,
I have also experienced this! When there is no code in the processor, it will automatically go into bootloader mode, that is why you can load first time.
I don't think the problem is flash Magic, but the RESET pin on the processor is not being seen.
I have also made a post to see if anyone is aware of a RESET issue.
Thanks
0 件の賞賛
返信