LPC2294 External Flash Read and Write

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2294 External Flash Read and Write

1,689 次查看
1263906294
Contributor I
  • i use software "JFlash" to program on external flash, but there is an error "programming failed @address 0x80000000 ". there is nothing wrong when erasing and reading back, but the pin WE is always high while programming. could you tell me the reason? The picture of JFLASH is as follow:
  • 微信图片_20170613174200.jpg
标签 (1)
0 项奖励
回复
1 回复

1,419 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Most of the times, it would be required to generate a proper configuration file according to the used external memory. You could take a look at the following links, that may provide useful related information, depending of the hardware, IDE and debug tool:

https://www.lpcware.com/content/forum/help-j-link-program

https://www.embeddedrelated.com/showthread/lpc2000/8706-1.php

http://www.keil.com/forum/6027/

http://forum.segger.com/index.php?page=Thread&threadID=20

https://www.embeddedrelated.com/showthread/lpc2000/35484-1.php

https://www.lpcware.com/content/forum/need-help-programming-external-flash-lpc-link2-board


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复