LPC2294 External Flash Read and Write

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2294 External Flash Read and Write

1,613 次查看
1263906294
Contributor I

is there a interface module controlling LPC2294 to read and write external flash?

now i wanna write a data into external flash,how can i put it on the address bus? via something like a spercific register, or set the address pin as GPIO to pull up and pull down

标记 (2)
0 项奖励
回复
1 回复

1,498 次查看
CarlosCasillas
NXP Employee
NXP Employee

 Hi,

Most of the times, it would be required to generate a proper configuration file according to the used external memory. You could take a look at the following links, that may provide useful related information, depending of the hardware, IDE and debug tool:

https://www.lpcware.com/content/forum/help-j-link-program

https://www.embeddedrelated.com/showthread/lpc2000/8706-1.php

http://www.keil.com/forum/6027/

http://forum.segger.com/index.php?page=Thread&threadID=20

https://www.embeddedrelated.com/showthread/lpc2000/35484-1.php

https://www.lpcware.com/content/forum/need-help-programming-external-flash-lpc-link2-board

 
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复