LPC2294 External Flash Read and Write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2294 External Flash Read and Write

1,704 Views
1263906294
Contributor I
  • i use software "JFlash" to program on external flash, but there is an error "programming failed @address 0x80000000 ". there is nothing wrong when erasing and reading back, but the pin WE is always high while programming. could you tell me the reason? The picture of JFLASH is as follow:
  • 微信图片_20170613174200.jpg
Labels (1)
0 Kudos
Reply
1 Reply

1,434 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Most of the times, it would be required to generate a proper configuration file according to the used external memory. You could take a look at the following links, that may provide useful related information, depending of the hardware, IDE and debug tool:

https://www.lpcware.com/content/forum/help-j-link-program

https://www.embeddedrelated.com/showthread/lpc2000/8706-1.php

http://www.keil.com/forum/6027/

http://forum.segger.com/index.php?page=Thread&threadID=20

https://www.embeddedrelated.com/showthread/lpc2000/35484-1.php

https://www.lpcware.com/content/forum/need-help-programming-external-flash-lpc-link2-board


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply