LPC2294/01 CAN Rx Failure on Data Overload

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2294/01 CAN Rx Failure on Data Overload

3,199件の閲覧回数
mikesfn
Contributor III

First some background....

I'm running an LPC2294/01 with a CAN bus connection to an external PC running CAN simulation software (Vector CANalyzer/CANoe). The problem I've been encountering is as follows: when the unit (LPC2294) is off and the simulator is running (ie. attempting to transmit data to the unit), the unacknowledged messages are buffered into a queue of some fixed size (I do not have control over this behavior). When the unit is then powered on and initializes its CAN controller (SJA1000), the simulator then barfs that queued data onto the bus as fast as the controller will ACK it, before continuing with the fixed-period real-time data. This often leads to a Data Overrun fault since the software does not expect this sudden dump at the beginning and therefore does not sample the receive registers fast enough. After this occurs, the CAN controller no longer signals any incoming/received data to the software (CANGSR RBS bit stays 0), despite continuing to ACK those incoming messages. After much searching I found the Errata document for this microcontroller (ES_LPC229x/01) which explained the issue as follows:

"

Problem:

In a Data Overrun condition, the CAN controller is locked from further message reception.

Work-around:

1. Recovering from this situation is only possible with a soft reset to the CAN controller.

...

"

Taking the advice, I updated the software to reset the CAN controller upon detection of the Data Overrun (based on the CANGSR DOS bit). This helped significantly, but it still was not a 100% fix. The behavior described in the Errata where the CAN Rx buffer is locked from receiving any new data still happens occasionally with no indication of data overrun in any of the controller registers. It's not clear to me if something else is going on. So, this becomes a two part question:

1) Is it possible for the scenario described in the Errata (ES_LPC229x/01 section 3.2), to occur even if no data overrun is signaled by the corresponding register bits (either CANGSR DOS, or CANICR DOI)?

2) If the answer above is 'Yes', is there another work around besides increasing the sampling rate? The acceptance filter is already configured to pass through only valid data. The problem occurs when multiple instances of these valid IDs are received much faster than their expected period.

Any ideas are appreciated.

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,866件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Michael,

Your issue was internally escalated. I will post an update as soon as having news. I have also provided your additional information sent by the Case.

Best regards!

/Carlos

0 件の賞賛
返信

2,866件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Michael,

There are no previous reports of CAN buffer lock up without overrun.

Could you try increasing CAN receive interrupt routine to higher priority to rest of code to ensure that reception is instant.

 

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信