LPC2292FBD144/01.5 is not recommended for new design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2292FBD144/01.5 is not recommended for new design

1,093 Views
vikhyatbaxi
Contributor I

Hi 

 

LPC2292FBD144/01.5 is not recommended for new design.

1. Can you suggest alternate pin to pin replacement with more code memory ?

2. Can you also suggest alternate microcontroller of similar family with added feature and more code memory?

 

 

 

0 Kudos
Reply
3 Replies

1,085 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI vikhyatbaxi 

We have pin to pin replacement LPC177x/8x for LPC23xx and LPC24xx but not replacement for LPC21xx/22xx.

If you want, please send me your requirement. Flash/RAM size, CPU frequency, necessary peripherals needed. I can help you look for a replacement. but please note, not pin to pin replacement.

Thanks,

Jun Zhang

0 Kudos
Reply

1,075 Views
vikhyatbaxi
Contributor I

Hi 

It is running production design changes, thus

 

Option1 :

We would like to keep Micro family similar if we can not find pin-pin replacement, micro frequency similar

1. Family : ARM7 same as LPC2292FBD144/01.5

2.Core Size : 32bit same as LPC2292FBD144/01.5

3. Speed : 60MHz  same as LPC2292FBD144/01.5

4. Connectivity : > = 1 CANbus, EBI/EMI, >=1 I²C, Microwire, >=1 SPI, SSI, SSP, >=1 UART/USAR

5. Peripherals : POR, PWM, WDT

6. No of IO >= 112

7. Program memory >= twice the current memory 256KB (256K x FLASH

8. RAM size >= twice the current size 16K x 8

9. A/D >= 8x10b i.e 12-bit preferred.

Option2 : New micro family with above minimum requirement which will require significant amount of work and as it is running production change we may not proceed with option2.

0 Kudos
Reply

1,071 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

Thanks, please check LPC546xx. it may match your requirement. It is function replacement but not pin-to-pin replacement.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

If this can't help, please let me know.

Jun Zhang

0 Kudos
Reply