LPC2148 with emWin_512_ARM7TDMI_LE.LIB issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2148 with emWin_512_ARM7TDMI_LE.LIB issue

846 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Jat on Mon Apr 09 09:47:47 MST 2012
i have a custom designed board running a 800x600 LCD directly from LPC2148. The SWIM library is running great with the design but when I tried to include the NXP emWin library that is avaliabel on LPCWare "emWin_512_ARM7TDMI_LE.LIB", the program stops at the "GUI_Init()".

after stepping through the program, I found that the functions "LCD_SetSizeEx" and "LCD_SetVSizeEx" are returning "1" and the emWin datasheet mentions that these functions should return "0" when successful.


Can someone please help on how to use LPC2148 with emWin_512_ARM7TDMI_LE.LIB.


Thanks
标签 (1)
0 项奖励
回复
0 回复数