LPC2138FBD64/01,15 compatibility with LPC2138FBD64/01EL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2138FBD64/01,15 compatibility with LPC2138FBD64/01EL

Jump to solution
2,436 Views
mattiad
Contributor I

Dear All,

 

I’m using the microcontroller NXP LPC2138FBD64/01,15 and I discovered that now it’s considered obsolete. I’ve found the alternative LPC2138FBD64/01EL which seems essentially the same but I don’t have the effective visibility which they are totally compatible.

Has anyone any document which explains the difference between these two codes?

 

Best Regards,

 

Mattia

0 Kudos
Reply
1 Solution
2,426 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Mattiad,

I copy the screenshot here

Regard

XiangJun Rong

xiangjun_rong_0-1599113241705.png

 

View solution in original post

0 Kudos
Reply
2 Replies
2,426 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport
 
 
 

 

 

 

Hi, Mattiad,

I think that the LPC2138FBD64/01, 11 and LPC2138FBD64/01, 15 and LPC2138FBD64/01EL are the same, the difference is the package. For the 151 index, the package is TRAY-TRAY, for the 11 index, the package is reel-reel, for the 15, it is TRAY-TRAY single.

Hope it can help you

BR

XiangJun Rong

 

 

 

 

 

 

 

 

 

 

 

 

 

 

0 Kudos
Reply
2,427 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Mattiad,

I copy the screenshot here

Regard

XiangJun Rong

xiangjun_rong_0-1599113241705.png

 

0 Kudos
Reply