LPC2136 startup problem after jtag flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2136 startup problem after jtag flash

902件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhall0819 on Mon Jun 09 05:10:04 MST 2014
Hi

I have a LPC2136 based design. I develop with IAR and J-Link. Production programming used Segger J-Flash.
This design has been trouble free for years but a recent firmware upgrade has a strange problem.

A production unit is programmed with the Segger J-Flash. The code starts but resets almost immediately.
BUT when I connect the J-Link without the IAR IDE running (just the J-Link plugged in) the problem goes away and all is well forever after?

Any thoughts?

Thanks
ラベル(1)
0 件の賞賛
返信
0 返答(返信)