LPC2134 SVD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2134 SVD

1,488 Views
Tomlinson
Contributor I

Hello, I was wondering if anyone knew where to get SVD files for the LPC2134 mcu? I found one project online that linked an SVD in a PAC but it was for LPC176x5x_v0.2.svd. Any help would be appreciated!

0 Kudos
Reply
3 Replies

1,456 Views
Harry_Zhang
NXP Employee
NXP Employee

HI @Tomlinson 

You can refer to it LPC2468 - NXP Community

 

BR

Hang

0 Kudos
Reply

1,438 Views
Tomlinson
Contributor I

Are there any peripheral/register definition files of any sort available at all?

0 Kudos
Reply

1,401 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Tomlinson 

Sorry, there are no peripheral/register definition files of any sort available.

But you can use a similar SVD,  If you found an SVD file for the LPC176x family, there might be enough overlap in peripheral functionality that you can use it as a base, and tweak any differences manually. Be careful with differences in peripherals, as the two MCUs are from different families.

BR

Hang

 

0 Kudos
Reply