LPC2129FBD64 Bootloader version 1.65 to 1.70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2129FBD64 Bootloader version 1.65 to 1.70

1,753件の閲覧回数
engsayeed
Contributor I

Dear All,
we are facing some issue in  LPC2129FBD64. i have LPC2129FBD64 bootloader version 1.65 IC program hex file. now i buy new LPC2129FBD64 but this ic bootloader version is 1.70. program upload is done but program not work properly and very slow run. please give me solution.

ラベル(1)
0 件の賞賛
返信
1 返信

1,721件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport
1. How did you update bootloader from 1.65 to 1.70? Is it possible to revise it back to confirm if the problem was caused by different bootloader version?
2.  I didn't see any existing report for bootloader 1.70. So to position the issue, please do some test:
- test it with a simple demo code, for example, toggle a led. Is it work normal on both 1.65 and 1.70?
- test system clock. Are both of them the same system clock?
- which module can't work normal on 1.70?
 
Have a nice day
Jun Zhang
0 件の賞賛
返信