LPC2129FBD64 Bootloader version 1.65 to 1.70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2129FBD64 Bootloader version 1.65 to 1.70

1,695 Views
engsayeed
Contributor I

Dear All,
we are facing some issue in  LPC2129FBD64. i have LPC2129FBD64 bootloader version 1.65 IC program hex file. now i buy new LPC2129FBD64 but this ic bootloader version is 1.70. program upload is done but program not work properly and very slow run. please give me solution.

Labels (1)
0 Kudos
Reply
1 Reply

1,663 Views
ZhangJennie
NXP TechSupport
NXP TechSupport
1. How did you update bootloader from 1.65 to 1.70? Is it possible to revise it back to confirm if the problem was caused by different bootloader version?
2.  I didn't see any existing report for bootloader 1.70. So to position the issue, please do some test:
- test it with a simple demo code, for example, toggle a led. Is it work normal on both 1.65 and 1.70?
- test system clock. Are both of them the same system clock?
- which module can't work normal on 1.70?
 
Have a nice day
Jun Zhang
0 Kudos
Reply