LPC2106 timer0 match interrupt without reset counter not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2106 timer0 match interrupt without reset counter not work

1,058 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hydromet on Tue Nov 18 22:49:30 MST 2014
I need periodic interrupts with T0TC from 0 to 0xffffffffL
    PINSEL0_bit.P0_4=2;              // select Pin P0.4 as CAP0.1
  T0TCR = 2;
  T0CTCR = 0; // Set timer counters mode - clock by PCLK
T0PR  = 0;     // Set timer prescaler
T0MR0 = 3600;// Set timer period
  T0MCR = 1;  // Set match action - interrupt by MR0 enable without reset counter
        T0CCR = 0x38;    //Set timer counters mode - clock by CAP0.1 (8 - rising edge, 0x10 - falling edge, 0x20 - interrupt)                                 // 0x38 = (5 << 3) - rising
  T0EMR = 0;
  VICIntSelect &= ~(1<<VIC_TIMER0); 
  VICVectAddr0 = (_U32) Tmr0IntOnMR0_isr;
  VICVectCntl0 = 0x20 | VIC_TIMER0;
  VICIntEnable |= (1<<VIC_TIMER0);
  T0TCR = 1;
....................................................................
__irq __arm void Tmr0IntOnMR0_isr(void){
  if(T0IR_bit.MR0INT){
// clear interrupt flag
T0IR_bit.MR0INT = 1;
    T0MR0 += 3600;
.......................................
  }
  if(T0IR_bit.CR1INT){
T0IR_bit.CR1INT = 1;
   PINSEL0_bit.P0_4=0;               // select Pin P0.4 as GPIO
IODIR_bit.P0_4 = 0;
if(IOPIN_bit.P0_4){
........................................
}
else {
........................................
}
   PINSEL0_bit.P0_4=2;               // select Pin P0.4 as CAP0.1
  }
  VICVectAddr = 0;
}
Labels (1)
0 Kudos
Reply
0 Replies