LPC18S50. How to load an empty external flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC18S50. How to load an empty external flash

3,066 Views
angelmelendez
Contributor I

How can be an empty external flash loaded in circuit

Labels (1)
0 Kudos
Reply
5 Replies

2,742 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Another alternative : use the the LPCScrypt utility to download directly into flash via USB - http://www.nxp.com/lpcscrypt

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

2,742 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Angel!

Could you please provide more information of what you are trying to do. Are you trying to erase the external flash?

Have a great day!

Victor

0 Kudos
Reply

2,742 Views
angelmelendez
Contributor I

Dear Victor.

I'm worried about how to load the programs into the flash memories (SPI

Flash and/or Parallel NOR Flash) during the manufacturing process.

I think that this could be done using Flash Magic and/or Ulink and MDK

Keil. Is this right?.

I think that for using Flash Magic, I should use USART0. But USART0 pines

are ocupied for Address signal. I prefer to keep the integrity of the

address bus for better electrical performance. Then, is it better to use

Ulink+Keil MDK?.

Thanks. Best regards.

Angel

2018-03-21 18:24 GMT+01:00 victorjimenez <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: LPC18S50. How to load an empty external flash

reply from Victor Jimenez

<https://community.nxp.com/people/victorjimenez?et=watches.email.thread>

in LPC - View the full discussion

<https://community.nxp.com/message/997861?commentID=997861&et=watches.email.thread#comment-997861>

0 Kudos
Reply

2,742 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Angel,

According to the reference manual of the LPC18S50 (UM10430) you can also the use the USART3 for using flash magic, please reference chapter 5 page 56 section FEATURES.

 If you want to load the programs from the JTAG instead of bootloader you can do this using the command line of LPCXpresso/MCUXpresso. Please refer to the next post to see how to do this:

Using the command line flash programming tool 

Also, the option you mentioned Ulink + Keil MDK  is a good choice, I just wanted to give you more options!

Hope it helps!

Victor Jimenez.

0 Kudos
Reply

2,742 Views
angelmelendez
Contributor I

Hello Victor,

Thanks once again.

I'll try all your recommendations.

Then, I'll decide what of them will be the most suitable for developing and for manufacturing.

Best regards.

Angel Melendez

0 Kudos
Reply