LPC18S37 evaluation board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC18S37 evaluation board

1,522件の閲覧回数
haulam
Contributor II

I want to use chip LPC18S37 for AES hw encryption + USB MSC and SD Card.

Do we have any EVK which support all that features.

ラベル(2)
0 件の賞賛
返信
1 返信

1,393件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Hau,

The next board LPCXpresso18S37 Development Board|NXP  has the LPC18S37 chip, AES hw encryption and USB MSC. You are only missing the SD Card, but you can use the following general purpose shield LPC General Purpose Shield for LPCXpresso boards|NXP  that has the SD Card and it's compatible with the EVK mentioned before. 

Hope it helps!

Victor.

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------