LPC18S37 evaluation board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC18S37 evaluation board

1,487 Views
haulam
Contributor II

I want to use chip LPC18S37 for AES hw encryption + USB MSC and SD Card.

Do we have any EVK which support all that features.

Labels (2)
0 Kudos
Reply
1 Reply

1,358 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Hau,

The next board LPCXpresso18S37 Development Board|NXP  has the LPC18S37 chip, AES hw encryption and USB MSC. You are only missing the SD Card, but you can use the following general purpose shield LPC General Purpose Shield for LPCXpresso boards|NXP  that has the SD Card and it's compatible with the EVK mentioned before. 

Hope it helps!

Victor.

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------