LPC1857- stepping up/down PLL speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1857- stepping up/down PLL speed

798 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vivien.wong on Sun Jan 31 22:08:43 MST 2016
Hi there,

  I'm using the LPC1857 and I'm running at 96MHz with a clk in crystal of 12MHz. At some point of the code I wish to step up to 180MHz for higher performance and when that is done, i want to step back down to 96MHz. What is the best way to do this? Right now, i'm setting it this way:

   void SystemSetClockRateOptimalCurrent()
{
/* Setup PLL for maximum clock */
Chip_Clock_SetupMainPLLHz(CLKIN_CRYSTAL, CRYSTAL_MAIN_FREQ_IN, CLOCK_FREQ_LOW, CLOCK_FREQ_LOW);
Chip_Clock_SetBaseClock(CLK_BASE_MX, CLKIN_MAINPLL, true, false);

Chip_CREG_SetFlashAcceleration(CLOCK_FREQ_LOW);
}

void SystemCoreClockUpdate(void)
{
/* CPU core speed */
SystemCoreClock = Chip_Clock_GetRate(CLK_MX_MXCORE);
}


  Do i just setup for 180MHz and update the system core clock and then setup for 96MHz and do the same? Is there a better way in doing this?

Thanks
Regards
Vivien
标签 (1)
0 项奖励
回复
0 回复数