LPC1857 on Keil MCB1800 Dev Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1857 on Keil MCB1800 Dev Kit

Jump to solution
1,997 Views
sanders7284
Contributor III

Hello I have purchased a Keil1800 Dev PCB

I have downloaded the IAR examples from

LPCOpen Software for LPC18XX|NXP 

But I can only get the simple blinky and pherif examples to run

The emWin examples and example that use the emc won't run. (which is what i actually want the dev kit for).

there seem to be missing libaries etc

I downloaded Keil uVision and get the same results 

If you could advise on how to reslove the above or can point me to any other examples of emWin and emc for LPC1857 that would be great.

Cheers Paul

1 Solution
1,833 Views
bernhardfink
NXP Employee
NXP Employee

You may need to download the emWin libraries seperately. 

http://www.nxp.com/pages/emwin-graphics-library:EMWIN-GRAPHICS-LIBRARY?fsrch=1&sr=1&pageNum=1

Due to our license agreement we can't bundle this with our software package. 

The emWin Statup Guide should provide enough information for the installation into your environment.

Regards.

View solution in original post

2 Replies
1,834 Views
bernhardfink
NXP Employee
NXP Employee

You may need to download the emWin libraries seperately. 

http://www.nxp.com/pages/emwin-graphics-library:EMWIN-GRAPHICS-LIBRARY?fsrch=1&sr=1&pageNum=1

Due to our license agreement we can't bundle this with our software package. 

The emWin Statup Guide should provide enough information for the installation into your environment.

Regards.

1,833 Views
sanders7284
Contributor III

Thank you Bernhard,

I now have the graphics working!

Regards Paul Sanders

0 Kudos
Reply