LPC1857 on Keil MCB1800 Dev Kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1857 on Keil MCB1800 Dev Kit

ソリューションへジャンプ
1,992件の閲覧回数
sanders7284
Contributor III

Hello I have purchased a Keil1800 Dev PCB

I have downloaded the IAR examples from

LPCOpen Software for LPC18XX|NXP 

But I can only get the simple blinky and pherif examples to run

The emWin examples and example that use the emc won't run. (which is what i actually want the dev kit for).

there seem to be missing libaries etc

I downloaded Keil uVision and get the same results 

If you could advise on how to reslove the above or can point me to any other examples of emWin and emc for LPC1857 that would be great.

Cheers Paul

タグ(4)
1 解決策
1,828件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

You may need to download the emWin libraries seperately. 

http://www.nxp.com/pages/emwin-graphics-library:EMWIN-GRAPHICS-LIBRARY?fsrch=1&sr=1&pageNum=1

Due to our license agreement we can't bundle this with our software package. 

The emWin Statup Guide should provide enough information for the installation into your environment.

Regards.

元の投稿で解決策を見る

2 返答(返信)
1,829件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

You may need to download the emWin libraries seperately. 

http://www.nxp.com/pages/emwin-graphics-library:EMWIN-GRAPHICS-LIBRARY?fsrch=1&sr=1&pageNum=1

Due to our license agreement we can't bundle this with our software package. 

The emWin Statup Guide should provide enough information for the installation into your environment.

Regards.

1,828件の閲覧回数
sanders7284
Contributor III

Thank you Bernhard,

I now have the graphics working!

Regards Paul Sanders

0 件の賞賛
返信