LPC1857 SPIFI support MX25L51245G?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1857 SPIFI support MX25L51245G?

1,682 Views
billsheng
Contributor II

Currently, we're using Spansion S25FL256S(256Mbit) via LPC1857 SPIFI interface.

We are going to use a 512Mbit QSPI flash, unfortunately, S25FL512 has no WSON-8 footprint.

We found MXIC MX25L51245G has pin compatible one with WSON-8 footprint.

We changed the flash loader memory setup, with IAR J-Link, there just reported error without additional information.

With DFUSec tool, there reported PROGRAM CYCLE ERROR, details log are in the attachment.

I'm wondering that whether LPC1857 SPIFI support MX25L51245G.

Looking forward to get some confirmation from NXP.

 

Original Attachment has been moved to: output.log.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,432 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Bill Sheng,

I'm afraid the MX25L51245G is not supported now, it's too large.

pastedImage_1.png


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply