LPC1857 SPIFI (XIP functionality)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1857 SPIFI (XIP functionality)

1,422 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nesrine on Mon Feb 23 05:24:04 MST 2015
Hi,
I use the Keil MCB1857 board,
I would to execute my code from SPI flash(SPIFI),my board include S25FL256SAGMFI001 memory.
My question is about the  implementation of the  execute in place (XIP)  functionality in your architecture,because i found anything in the documentations.
Thank you
Nesrine
Labels (1)
0 Kudos
Reply
2 Replies

1,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nesrine on Tue Feb 24 08:50:59 MST 2015
Hi,
thank you for the response,
my program work well,but i would know more about the implementation ,
if you use the SDR or the DDR mode?
if you implement the XIP functionnality?
the frequency of the SPIFI (DIVA?) why the use of the DIVA?
The lengh of the ,Cache prefetching?
i have many questions but i found anything in documentation!!
thank you
Nesrine
0 Kudos
Reply

1,336 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Feb 23 11:40:00 MST 2015
Hi nesrine,
Boot loader and SPIFI library will take care of XIP.
Please set your boot jumper to boot from SPIFI. Erase internal flash and run below example. This example is developed for LPCxpresso IDE.

Please use flash driver from below link.
http://www.lpcware.com/system/files/LPC18_43_SPIFI_8MB_64KB-New.zip

Let us know your feedback.
0 Kudos
Reply